Technical FAQs

Ask a Question

The I-Line interior HCM23734M uses an LA36400 breaker as a main. Can an LC36400 breaker be installed as a main to raise the AIC rating of the panel?

The LA main breaker in the HCM panel cannot be changed to an LC type. There is not enough room on the main breaker pan for the LC type breaker.


CTA-ID : 2037562
Was this helpful?
What can we do to improve the information ?