Technical FAQs

Ask a Question

What is the diameter of the shaft of the 9007C limit switch?

Issue:
Need to know the size and diameter of the shaft

Product Line: 
Limit Switches

Environment:
North American Products

Cause:
​Would like to know the diameter so they can plan how the switch is going to be mounted.

Resolution:

9007C•••• A, B, C, N, T5, T10 heads have the same shaft diameter of 0.44in or 11mm.
The drawing is on Digest 177 page 21-35


 
Was this helpful?
What can we do to improve the information ?