Technical FAQs

Ask a Question

What is the part number for the cable provided in the VW3A31101 Keypad remote mount kit?

The cable is not available as a separate item. It is only available as a kit which includes the keypad, mounting hardware and a 3 meter cable.

CTA-ID : 2036522
Was this helpful?
What can we do to improve the information ?