Technical FAQs

Ask a Question

Are the base mounting holes the same pattern with the XVE as with the XVA ?

No . There are no holes in the base of the XVE and there would be no room to drill any. The XVE Must be used with a XVBZ --mounting base because the opening is setup for the throat of that base. The set screw in the XVEC21 tightens over that throat.

CTA-ID : 2037421
Was this helpful?
What can we do to improve the information ?