Technical FAQs

Ask a Question

What is the difference between an 9037EG8 and 9037EG9

The difference between these two devices is the range of float traval. The position range that the float can travel in See 9034CT9701 pages 36 to 39


CTA-ID : 2037528
Was this helpful?
What can we do to improve the information ?