Technical FAQs

Ask a Question

What fuse clips will be required if the fuse size increases for 5kV HVL/cc switch?

There are 2 different materials used for the HVL/cc fuse clips. The size of the clip remains the same but the material changes. For 5kV fuses up to 200E the clip is phosphor bronze. For 15kV fuses up to 100E the clip is phosphor bronze. The bronze clip part number is 44044-042-01. Fuses above these ratings require a clip made of Beryllium part number 44044-042-02.

CTA-ID : 2037428
Was this helpful?
What can we do to improve the information ?