Technical FAQs

Ask a Question

What is the part number of the cover screws use on the SDAG26 auxiliary gutter?

Issue:
Current design repair parts

Product Line:
QO load centers

Environment:
Repair parts

Issue:
Maintenance

Resolution:
The part # for the Cover screws is 4020513002K (bag of 10 screws). These are the same screws used on standard QO load center covers.


CTA-ID : 2037398
Was this helpful?
What can we do to improve the information ?