Technical FAQs

Ask a Question

Are external current transformers provided as standard with the Motor Logic Plus overload relays?

No, the CT`s, if required, must be purchased separately.

Note: CT`s selected must provide 1% accuracy. See document 4210CT9701

CTA-ID : 2037689
Was this helpful?
What can we do to improve the information ?