Technical FAQs

Ask a Question

On an NQOD 400A panel using an LAL36400 main breaker, is there a main breaker cover available that has a slot for accessing the magnetic trip control?

There is no main breaker adapter kit cover that has a slot for accessing and changing the magnetic trip setting. Magnetic trip settings on main breakers are usually set only once, in most circumstances. The main breaker adapter kit front covers have a rectangular opening for the breaker throw only.

CTA-ID : 2037632
Was this helpful?
What can we do to improve the information ?