Technical FAQs

Ask a Question

What wire sizes will the QON442MS400 load center accommodate?

The lugs will accept one conductor ranging in size from #4 through 600kcmil or two conductors ranging in size from #4 through 250kcmil.


CTA-ID : 2037467
Was this helpful?
What can we do to improve the information ?