Technical FAQs

Ask a Question

Are the 9070SK type Transformer Disconnects available in Nema 4X enclosures?

Issue:
Enclosure ratings for 9070SK Transformer Disconnects

Product Line:
LV Transformers

Environment:
Applies to 9070 Class Transformer Disconnects by SquareD/Schneider Electric

Cause:
9070SK Transformer Disconnects are potentially used in different environments

Resolution:

No. The 9070SK type Transformer Disconnects are available in NEMA 1 and NEMA 12 type enclosures only.


CTA-ID : 2037592
Was this helpful?
What can we do to improve the information ?