Technical FAQs

Ask a Question

What is the coil burden for Integral 18, Integral 32 and Integral 63 Starters?

Integral 18:
Inrush: AC - 75VA (50hz); 90VA (60hz)
Sealed: AC - 8VA (50hz); 9VA (60hz)
Inrush: DC with converter - 100 watts
Sealed: DC with converter - 1.5 watts
Integral 32:
Inrush: AC - 160VA (50hz); 185VA (60hz)
Sealed: AC - 12VA (50 or 60 hz)
Inrush: DC with converter - 250 watts, duration 50 ms
Sealed: DC with converter - 4 watts
Integral 63:
Inrush: AC - 375VA (50hz); 450VA (60hz)
Sealed: AC - 25VA (50 or 60hz)
Inrush: DC with converter - 300 watts, duration 50 ms
Sealed: DC with converter - 8 watts.



CTA-ID : 2037511
Was this helpful?
What can we do to improve the information ?