Technical FAQs

Ask a Question

What replaced the EZM, 200amp meter socket branch devices, for example the EZM113200?

Issue:
Product replacement

Product Line:
EZM Metering equipment

Environment:
Branch devices

Cause:
Application

Resolution:
The older 200amp meter socket EZM branch devices were replaced with 225amp meter socket branch devices. The EZM113200 was replaced with the EZM113225. The previous 200A branch devices went obsolete in late 2006 when the QE-VH plug-in style of tenant circuit breaker line was replaced by the new QDP-TM style of bolt-on circuit breakers.



CTA-ID : 2037479
Was this helpful?
What can we do to improve the information ?