Technical FAQs

Ask a Question

Can a NEMA Type 12 Heavy Duty Safety Switch be used in a dusty environment?

Issue:
Application

Product Line:
HD SS 

Cause:
NEMA Type Protection

Resolution:
Yes, a NEMA Type 12 device would be considered dust proof.  See NEMA standard for full description of NEMA 12, link listed below.

https://www.nema.org/Products/Documents/nema-enclosure-types.pdf

CTA-ID : 2037652
Was this helpful?
What can we do to improve the information ?