Technical FAQs

Ask a Question

What is the maximum amperage branch mounted backfed generator breaker that can be installed in an RC816F200C with the RCGK2 generator kit?

100 ampere maximum.


CTA-ID : 2037897
Was this helpful?
What can we do to improve the information ?