Technical FAQs

Ask a Question

Are definite purpose 8911 starters available with bimetallic overloads ?

No , just melting alloy types . Use a NEMA starter or IEC starter if a bimetallic overload is required .


CTA-ID : 2039007
Was this helpful?
What can we do to improve the information ?