Technical FAQs

Ask a Question

What class of fuse can be used with QMB366MW?

Issue:
Application

Product Line:
QMB

Environment:
Application of fuses

Cause:
Clarification

Resolution:
It will accept Class H or K fuses as standard; Class J, R or T fuses with modification.  When using Class J fuses, QMB600J is also required. When using Class R fuses, QMB4060R is also required. When using Class T fuses, QMB600T6 is also required.


CTA-ID : 2038059
Was this helpful?
What can we do to improve the information ?