Technical FAQs

Ask a Question

What Tenant Service Disconnects can be use in an old style MP45125R meter center?

Issue:
Application

Product Line:
Obsolete MP

Environment:
Application

Cause:
Selection of correctly applied tenant breakers

Resolution:
The MP45125R device will accommodate (5) 2-Pole Tenant Circuit Breakers of the following types and ampere rating ranges:
QO240 to QO2125 for 10kA SCCR (40A to 125A)
QO240VH to QO2125VH for 22kA SCCR (40A to 125A)
QOH240 to OH2125 for 42kA SCCR (40A to 125A)


CTA-ID : 2037929
Was this helpful?
What can we do to improve the information ?