Technical FAQs

Ask a Question

Does Square D/Schneider Electric offer Energy Efficient Transformers with lower dB levels, which is a lower overall sound level?

Transformers are often placed in quiet areas such as Libraries, Churches, and Offices. 

Product Line:
LV Transformers

Applies to Ventilated Energy Efficient Transformers from SquareD/Schneider Electric

Standard Transformers can produce amounts of noise that are objectionable in some installations

Yes. Energy Efficient Transformers are now available from Square D/Schneider Electric with 3dB or 6dB below standard sound levels and may be selected on the Transformer Product Selector Tool in Electronic Quote Management (EQM).

CTA-ID : 2038565

Was this helpful?
What can we do to improve the information ?