Technical FAQs

Ask a Question

What Class of fuse does the H328N, H328NR and H328NAWK safety switches accept?

Issue:
Product design features

Product Line:
Heavy Duty Safety Switches

Environment:
Fuses

Cause:
Installation

Resolution:
These switches accept Class L fuses ONLY. With Class L fuses installed, the switches are UL listed for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.

NOTE: The 600V type L fuses may be used in these 240Vac switches, however, the switch itself maintains a rating of 240V MAX.


CTA-ID : 2038883
Was this helpful?
What can we do to improve the information ?