Technical FAQs

Ask a Question

What is the temperature rating of the 9080LBA363106 power distribution block?

The 9080LBA36106 temperature range is -40 to 302 degrees F or -40 to 150 degrees C.


CTA-ID : 2038544
Was this helpful?
What can we do to improve the information ?