Technical FAQs

Ask a Question

What breakers and meter sockets are used with catalog number EZML332400?

Issue:
Product Design Features  

Product Line:
EZM metering

Environment:
EZM branch Tenant breakers

Cause
Maintenance

Resolution:

This catalog number has several series numbers associated with it for the different Series with circuit breakers see below:
For the Series M01 the device was supplied with two factory installed 3-Pole, 400A, LAL36400 circuit breakers.
For the Series M02 the device was supplied with two factory installed 3-Pole, 400A, DJM32400E20 circuit breakers.
For the current Series M03 the device is supplied with two factory installed 3-Pole, 400A, LJL36400U31X circuit breakers.

Each tenant breaker is fed by a Class 320 Lever Bypass Type Meter Socket having a Jaw Release feature.

The LAL breakers were NOT adjustable.
The DJM breakers were supplied with an adjustable ampere rating ranging from 160A min. to 400A max.
The LJL breakers are supplied with an adjustable ampere rating ranging from 125A min. to 400A max.

 
Was this helpful?
What can we do to improve the information ?