Technical FAQs

Ask a Question

Can the N600SFBJ accept a two pole breaker?

Issue:
Can the N600SFBJ subfeed breaker kit accept a two pole breaker.

Product Line:
NF panelboards and Accessories

Environment:
Product Characteristics

Cause:
Two pole breaker installation in subfeed breaker kit.

Resolution:
Yes, a two pole Powerpact J breaker can be used. (NOTE:  The N600SFBJ was a subfeed breaker adapter kit for the older, Series 0 NF panelboards. It is now obsolete with
no replacement)


CTA-ID : 2038832
Was this helpful?
What can we do to improve the information ?