Technical FAQs

Ask a Question

Can a QOB2125, QOB2125VH or QOB2150VH be installed into an older style NQOB panelboard?

No, this circuit breaker did not exist until after NQOB was obsolete; therefore, it has not been tested and UL listed for use in the panelboard.

CTA-ID : 2038802
Was this helpful?
What can we do to improve the information ?