Technical FAQs

Ask a Question

80110-041-02 is the part number for a NQOD interior deadfront trim which is obsolete. The number is updated, what is the new number?

The old number was for the deadfront sheet metal only. The new number is: 80116-324-56. This revised number is the new package that includes the labels.


CTA-ID : 2038477
Was this helpful?
What can we do to improve the information ?