Technical FAQs

Ask a Question

What are the dimensions of the PK15GTA Equipment Ground Bar Kit?

Issue:
Dimensions

Product Line:
Load Center Accessory

Cause:
Dimensions

Resolution:
The PK15GTA is 0.3125" Wide x 0.437" High x 5.60" Long


CTA-ID : 2037474
Was this helpful?
What can we do to improve the information ?