Technical FAQs

Ask a Question

On circuit breaker HDL36150CSO with a 24VDC shunt trip, the terminals are marked C1 and C2. Which is plus and which is minus?

Typically, the C1 terminal is negative (common), and the C2 terminal is positive. However, the DC shunt trip will work when wired in either direction.


CTA-ID : 2037777
Was this helpful?
What can we do to improve the information ?