Technical FAQs

Ask a Question

Can the CQOE260GFINM be used on a 120/240 vac, single-phase, 3 wire load?

No, it can only be used on a two wire 240vac load that has no neutral. There is no load neutral connection.

CTA-ID : 2037763
Was this helpful?
What can we do to improve the information ?