Technical FAQs

Ask a Question

What size box is used with the NQOD442L400TFL in a main lug application?

Issue:
What size box is used with the NQOD442L400TFL in a main lug application?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Circuit breaker panelboards sold and supported in the USA.

Cause:
Selection of correct box for specific NQOD panelboard interior.

Resolution:
Note:  The NQOD panelboard line is now obsolete, replaced by NQ. Selection of this interior isby separate components. Refer to the current Digest for catalog number selection.






















CTA-ID : 2038860
Was this helpful?
What can we do to improve the information ?