Technical FAQs

Ask a Question

What is the correct order of series numbers for Homeline load centers, beginning with the most current?

Issue:
Current Design Series

Product Line:
Homeline load centers

Environment:
Current Repair parts  

Cause:
Maintenance

Resolution:
The current series is S04, , then S03, then S02, then S01, then Series 3, then Series 2, and then Series 1 would be the oldest for Homeline load centers. 


CTA-ID : 2038841
Was this helpful?
What can we do to improve the information ?