Technical FAQs

Ask a Question

9007MS options 12, 54, 55, 82 and 84 - are these side mounted or bottom mounted?<br /><br /><br />

The connector will come from bottom of housing. For side entry connectors, include 06, then 12, 54, 55, 82, or 84.


CTA-ID : 2038358
Was this helpful?
What can we do to improve the information ?