Technical FAQs

Ask a Question

Can a Mag Gard breaker be factory installed as a subfeed breaker in an NQOD panelboard?

No. MagGard breakers are not UL listed as an available subfeed breaker for installation in NQOD panelboards. Standard thermal magnetic breakers are the only type suitable for this application.


CTA-ID : 2038342
Was this helpful?
What can we do to improve the information ?