Technical FAQs

Ask a Question

Can Class J fuses be used in a PS4620 busway plug-in unit ?

Yes. The load base will need to be relocated to the Class J fuse location per the installation instructions.



CTA-ID : 2038556
Was this helpful?
What can we do to improve the information ?