Technical FAQs

Ask a Question

What is the layout format for an EZMR116125?

Refer to CAD Drawing Number 3124 for layout and dimensional information.
This branch unit is configured as a single wide 6-Position unit with all meters in a single row.


CTA-ID : 2038552
Was this helpful?
What can we do to improve the information ?