Technical FAQs

Ask a Question

How is the 9001K68 guard installed?

The ring nut of the mushroom operator is removed and discarded. The operator is pushed through the 30mm hole from the back of the panel and the guard is screwed on tightly from the front. The mushroom knob is pushed on and snapped into place.

CTA-ID : 2038653
Was this helpful?
What can we do to improve the information ?