Technical FAQs

Ask a Question

What is the height of the outer door for an HVL outdoor switch enclosure?

The base channel is 4`` high. The door is above the base channel, but the door stay rods protrude downward from the door. The door stay rod rod is 4.18`` above the ground.


CTA-ID : 2038649
Was this helpful?
What can we do to improve the information ?