Technical FAQs

Ask a Question

Does the top space of the 9001SKYP pendant ( used for a toggle switch or SK operator or pilot light ) need a closing plate if it is not used?

No, this position is closed out and must be knocked out or drilled out if used.


CTA-ID : 2038560
Was this helpful?
What can we do to improve the information ?