Technical FAQs

Ask a Question

Do the FAL, KAL, LAL and MAL circuit breakers have designated line and load terminals? Can they be reverse or back fed?

Product Line:
Circuit Breakers

Resolution:
The FAL, KAL, LAL and MAL circuit breakers themselves do not have designated line and load terminals, so they are ok to reverse feed, or back feed. These breakers comply with UL489.
(Check the enclosure in which they are installed for any marked restrictions.)
Was this helpful?
What can we do to improve the information ?