Technical FAQs

Ask a Question

What is the range of QO breaker amperages that can be interlocked with a QO2DTI Mechanical Interlock Attachment?

Issue:
Application

Product Line:
QO LC Accessory

Cause:
Application

Resolution:
The QO2DTI interlock will work with single and double pole QO type breakers in the range of 10A to 125A. It will not work with the two pole QO2150, QO2175 or QO2200 breakers, since those breakers have larger frames which take up four pole spaces.


CTA-ID : 2038397
Was this helpful?
What can we do to improve the information ?