Technical FAQs

Ask a Question

Does Square D offer Heavy Duty Safety Switches for either 200A or 400A with the Appleton, Crouse-Hinds or Hubbellock Receptacles?

Issue:
Product Design Features

Product Line:
Heavy Duty Safety Switches

Environment:
Cover design

Cause:
Application

Resolution:
No. The Heavy Duty Safety Switches using the Appleton, Crouse-Hinds or Hubbellock receptacles are ONLY available in 30A, 60A, and 100A.


CTA-ID : 2038817
Was this helpful?
What can we do to improve the information ?