Technical FAQs

Ask a Question

How do you mount a QOB3110VH, QOB3125VH, and QOB3150VH breaker into an NQOD panelboard?<br /><br />

First slide the connector assembly to expose the screw. Make the electrical connection to the bus connectors. Then slide the breaker over towards the center of the panel and push the mounting clips onto the mounting rail. To remove the breaker, reverse the procedure. For further mounting detail information refer to bulletin 48940-072-03.

These breakers were not tested for use in NQOB or 400A QO load center interiors.

Same for NQOD. - WH


CTA-ID : 2038663
Was this helpful?
What can we do to improve the information ?