Technical FAQs

Ask a Question

Can a utility meter socket be installed in a factory assembled NF panelboard?

Issue:
Can a utility meter socket be installed in a factory assembled NF panelboard?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
No. There is no provision in the design of NF panelboards for installation of utility metering. There are some electronic metering PowerLogic factory assembled options, however.


CTA-ID : 2038122
Was this helpful?
What can we do to improve the information ?