Technical FAQs

Ask a Question

Can a TVS2EMA24A be used in a single phase application?

3 phase Surge suppressors cannot be used in single phase applications. The diagnostics will not work , the window is different configuration , you would have a red light on all the time.

CTA-ID : 2038554
Was this helpful?
What can we do to improve the information ?