Technical FAQs

Ask a Question

Can a QO360 breaker be used as a main circuit breaker in a QO312L125G, three-phase, load center?

The QO360 breaker can be utilized as a main circuit breaker, if a PK3MB, retaining kit is used to secure the breaker to the Interior.

CTA-ID : 2038497
Was this helpful?
What can we do to improve the information ?