Technical FAQs

Ask a Question

How do you set an XMLB010A2S13 pressure switch for pressure?

There are two setting screws on the XLMB pressure switch. ....a red one for high pressure and a green one for the differential. Set the High pressure first. Both screws turn clockwise for increasing and counter-clockwise for decreasing. Set the Green screw last. You must have air pressure or some other available adjustable pressure medium applied to the pressure switch during setting.

CTA-ID : 2038067
Was this helpful?
What can we do to improve the information ?