Technical FAQs

Ask a Question

Can we provide an interior light on an indoor HVL switch with the stored energy mechanism (SEM)?

No. The SEM HVL switch requires additonal air clearance at the front of the switch enclosure. The light assembly would interfere with this clearance.

CTA-ID : 2038163
Was this helpful?
What can we do to improve the information ?