Technical FAQs

Ask a Question

How often and at what intervals does an XY2C** cable pull switch need to be supported?

The first cable support should be within 4 inches of the switch. It is recommended to space supports along the entire length of the cable at 6 to16 foot intervals. Cable supports ensure the transmission of the cable tension in the axis of the switch cam. The first one after the switch is mandatory for correct operation - 4 inches. Also, if pulleys are used to change the direction of the cable, cable supports at 4 inches before and after the pulley are mandatory. Use supports with 0.8 inches maximum height H with respect to the product mounting surface.


CTA-ID : 2038102
Was this helpful?
What can we do to improve the information ?