Technical FAQs

Ask a Question

On the 9050JCK off delay and one shot timers are terminals 6 and 7 jumpered internally?

Issue:
On the 9050JCK off delay and one shot timers are terminals 6 and 7 jumpered internally?

Product Line:
General Purpose Relay

Environment:
Square D General Purpose Plug-In JCK Relay

Cause:
Clarify the difference between the new and old versions of the JCK relays.                                            

Resolution:                                                                 
They were on older series timers, but not in the current series. With the advent of the power trigger units, the initiating circuit uses pins 5 and 7 for the power trigger. The standard units that require a dry contact to initiate use pins 5 and 6 for the initiating circuit.
 
Was this helpful?
What can we do to improve the information ?