Technical FAQs

Ask a Question

Can a shunt trip be field installed on a KA or KAL type breaker?

The shunt trip for KA, KC and KAL are factory installed only.
All electrical accessories for the KA type breakers are factory-installed only.


CTA-ID : 2036731
Was this helpful?
What can we do to improve the information ?