Technical FAQs

Ask a Question

What optional lugs are available for an LC36350 breaker?

The AL600LI7 accomodates (1) 500-750kcmil AL or CU
CU600LI7 accomodates (1) 500-750kcmil CU
CU600LI5 will work with wire range (2) 4/0 - 500kcmil CU.
AL600LI35 will work with wire range (2) #1 AWG- 350kcmil AL or CU
CU600LI35 will work with wire range (2) #1 AWG- 350kcmil CU


CTA-ID : 2036642
Was this helpful?
What can we do to improve the information ?